\

Diesel Exhaust Fluid (DEF)

View local pricing and inventory as well as place orders online.
  • Products
  • Reference
{imgAlt}

What is Diesel Exhaust Fluid (DEF)?

Diesel Exhaust Fluid (also known as AUS 32 and commonly referred to as AdBlue in Europe, Australia, and New Zealand) is a solution of solid urea dissolved in deionized water to produce a concentration that is 32.5% urea and 67.5% deionized water.

How DEF Works

Controlled amounts of the DEF solution are injected into the engine exhaust stream prior to the SCR catalyst. The temperature of the exhaust converts the urea in the DEF to ammonia. The ammonia and NOx in diesel exhaust react in the presence of the SCR catalyst to convert the NOx into nitrogen (N2) and water (H2O).

Typical properties of a DEF solution with 32.5% urea


PropertyTypical Value
pH9.5
Kinetic Viscosity at 25°C1.28 cSt
Surface Tension at 25°C65 mN/m, min.
Heat Capacity0.82 BTU/lb (°F)
Vapor Pressure Factor (relative to water)0.88

  • Caterpillar offers DEF in 2.5 gallon (9.5 liter) bottles for single use applications and in semi-bulk quantities 264 gallon (1000 liter) totes.
  • Any commercial DEF that meets the ISO 22241-1 specification is allowed for use in Cat® SCR equipped vehicles.